2020-02-18 3:07 PM
Hello,
I've faced some problems with setting up and sending data for STM32L496 Serial Audio Interface (I2S) using HAL functions from the PACK. Could you recommend some software examples or a sequence of actions?
Thanks,
Alex
Solved! Go to Solution.
2020-02-26 7:54 AM
Everything works fine now. It just takes some time to make it work.
Alex
2020-02-18 7:54 PM
What problems exactly?
What is PACK?
JW
2020-02-19 7:20 AM
I use the PACK 2.3.0. for the micro STM32L496 on the Nucleo-L496ZG board.
After SAI1_A initialisation using HAL_SAI_Init(&hsai_BlockA1), I tried to send data using
HAL_SAI_Transmit(&hsai_BlockA1, (u8*)&test_sai, countof(test_sai), HAL_MAX_DELAY).
Everything is supposed to be OK: PLLSAI1, clock selection, settings for SAI1, frame and slot settings, etc.
There is nothing on SAI1_A pins.
Thanks,
Alex
2020-02-24 11:26 AM
Hello,
I can set up SAI's pll, frame, slot parameters successfully. Unfortunately, there is some problem with sending data. When I use the function HAL_SAI_Transmit, I can see that FIFO is fully loaded with data, SAI is enabled using __HAL_SAI_ENABLE(hsai), but there is no data on the SD pin. I can see FS and SCK signals.
Does anybody have any ideas what could cause the problem?
Thanks,
Alex
2020-02-26 7:54 AM
Everything works fine now. It just takes some time to make it work.
Alex
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.