2021-11-27 12:44 PM
I just got an STM32 Nucleo 64 - F411RE.
The board has a crystal installed on the debugger, and a crystal oscillator on the board.
Do I need to install an external crystal in the provided space X3? and how can I do so?
It's my first time using STM32 I don't really know what to do.
I will be using the board with FREE RTOS to drive motors for a robotic arm.
Solved! Go to Solution.
2021-11-27 1:14 PM
No, you don't need to install a crystal. The 8MHz clock source coming from the ST-Link chip is driven by a crystal and is very accurate. Even if the crystal wasn't there, you could use the internal HSI clock source with decent accuracy.
2021-11-27 1:14 PM
No, you don't need to install a crystal. The 8MHz clock source coming from the ST-Link chip is driven by a crystal and is very accurate. Even if the crystal wasn't there, you could use the internal HSI clock source with decent accuracy.
2021-11-27 2:17 PM
Thanks a lot for your help
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.