2018-07-06 2:29 AM
Hello,
is the DMAMUX somehow involved when doing DMA MEM2MEM transfers? Is the value in the DMAMUX channel corresponding to the selectedMEM2MEM DMA channel irrelevant or must it be zero? I did not see MEM2MEN mentioned in the DMAMUX chapter of RM0432.
2018-07-09 8:29 AM
Hello
Bonnes.Uwe
,DMAMUX is only for peripherals and not memory to memory.
When a channel of DMA1 is programmed with DMA_CCRx.MEM2MEM=1, there is no hardware peripheral request.
So,
DMAMUX is not involved.
With Regards,
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.