2014-07-12 6:59 AM
While trying to track down my DMA2 stalling problem, I've tried to enable interrupts for things other than completion.
As a result, I notice that these two definitions:</p>
#define
</b>
DMA_FLAG_FEIF0 ((uint32_t)0x10800001)
#define
DMA_FLAG_DMEIF0 ((uint32_t)0x10800004)
set a bit that's listed as reserved in LISR for DMA2.
Surely the 8's are erroneous, and should be zeroes, looking at the documentation of the register.
#define
DMA_FLAG_FEIF0 ((uint32_t)0x10000001)
2014-07-12 7:09 AM
Does the library actually write these values to the register, or is it a more complicated encoding that the library is processing?
2014-07-12 7:59 AM
2014-07-12 8:32 AM
/**
* @brief Checks whether the specified DMAy Streamx flag is set or not.
* @param DMAy_Streamx: where y can be 1 or 2 to select the DMA and x can be 0
* to 7 to select the DMA Stream.
* @param DMA_FLAG: specifies the flag to check.
* This parameter can be one of the following values:
* @arg DMA_FLAG_TCIFx: Streamx transfer complete flag
* @arg DMA_FLAG_HTIFx: Streamx half transfer complete flag
* @arg DMA_FLAG_TEIFx: Streamx transfer error flag
* @arg DMA_FLAG_DMEIFx: Streamx direct mode error flag
* @arg DMA_FLAG_FEIFx: Streamx FIFO error flag
* Where x can be 0 to 7 to select the DMA Stream.
* @retval The new state of DMA_FLAG (SET or RESET).
*/
FlagStatus DMA_GetFlagStatus(DMA_Stream_TypeDef* DMAy_Streamx, uint32_t DMA_FLAG)
{
FlagStatus bitstatus = RESET;
DMA_TypeDef* DMAy;
uint32_t tmpreg = 0;
/* Check the parameters */
assert_param(IS_DMA_ALL_PERIPH(DMAy_Streamx));
assert_param(IS_DMA_GET_FLAG(DMA_FLAG));
/* Determine the DMA to which belongs the stream */
if (DMAy_Streamx <
DMA2_Stream0
)
{
/* DMAy_Streamx belongs to DMA1 */
DMAy
=
DMA1
;
}
else
{
/* DMAy_Streamx belongs to DMA2 */
DMAy
=
DMA2
;
}
/* Check if the flag is in HISR or LISR */
if ((DMA_FLAG & HIGH_ISR_MASK) != (uint32_t)RESET)
{
/* Get DMAy HISR register value */
tmpreg
=
DMAy
->HISR;
}
else
{
/* Get DMAy LISR register value */
tmpreg = DMAy->LISR;
}
/* Mask the reserved bits */
tmpreg &= (uint32_t)RESERVED_MASK;
/* Check the status of the specified DMA flag */
if ((tmpreg & DMA_FLAG) != (uint32_t)RESET)
{
/* DMA_FLAG is set */
bitstatus = SET;
}
else
{
/* DMA_FLAG is reset */
bitstatus = RESET;
}
/* Return the DMA_FLAG status */
return bitstatus;
}
2014-07-12 8:38 AM
While the bit you are complaining about does appear extraneous, the most plausible reason for them being there is to differentiate the encoding from others, and permit the assert_param() to catch bogus values.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.