2018-05-08 9:56 AM
Hi all, I have a STM32 NUCLEO-H743ZI evaluation board. I am trying to read ADC using DMA. Meanwhile, I also need to use the CPU to process the data read from the ADC. So I use a double buffer mode.
I used CubeMX to generate the framework of the code. Then I modified a bit to enable the double buffer mode. I tried to use the functions HAL_ADC_ConvHalfCpltCallback and HAL_ADC_ConvCpltCallback. However, seems like they are being called at the same frequency.
My question is: Can I get an interrupt when the Buffer1 is filled while Buffer 2 is being filled? If yes, is there any actions I should take?
My question is similar to this thread:
https://community.st.com/0D50X00009XkaF6SAJ
but I did not see a solution in that thread. I have the same needs:'Here's essentially what I'd like to happen:
1.) Buffer 0 fills
2.) interrupt occurs (I service Buffer 0)
3.) Buffer 1 fills
4.) interrupt occurs (I service Buffer 1)
5.) repeat 1 through 4'
null2018-08-10 9:41 AM
Sorry, bumping old zombie unanswered threads off my feed
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.