2021-10-14 2:33 AM
Hi All,
I want to use DMA to receive unknown length data. So I config USART_IT_IDLE and DMA_IT_TC and set DMA_BufferSize = 30 bytes. When the length of received data is less than 30 bytes, It works correctly and enters the USART1_IRQHandler(void) function. But the length of data is equal to 30 bytes, it enters the DMA1_Channel5_IRQHandler(void) function first then enters the USART1_IRQHandler(void) function again. Why does the length of data be equal to BufferSize cause Idle interruption?
void RCC_Configuration(void)
{
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_USART1 ,ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1,ENABLE);
}
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
GPIO_DeInit(GPIOA);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; // TX
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; // RX
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOA, &GPIO_InitStructure);
}
void USART_Configuration(void)
{
USART_InitTypeDef USART_InitStructure;
USART_DeInit(USART1);
USART_InitStructure.USART_BaudRate = 115200;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART1, &USART_InitStructure);
USART_Cmd(USART1,ENABLE);
USART_ITConfig(USART1,USART_IT_IDLE,ENABLE);
}
void DMA_Configuration(void)
{
DMA_InitTypeDef DMA_InitStructure;
DMA_DeInit(DMA1_Channel4);
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)(&USART1->DR);
DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)TxBuffer;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralDST;
DMA_InitStructure.DMA_BufferSize = 256;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte;
DMA_InitStructure.DMA_Mode = DMA_Mode_Normal;
DMA_InitStructure.DMA_Priority = DMA_Priority_VeryHigh;
DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;
DMA_Init(DMA1_Channel4, &DMA_InitStructure);
DMA_Cmd(DMA1_Channel4, ENABLE);
DMA_ITConfig(DMA1_Channel4,DMA_IT_TC | DMA_IT_TE,ENABLE);
DMA_DeInit(DMA1_Channel5);
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)(&USART1->DR);
DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)RxBuffer;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC;
DMA_InitStructure.DMA_BufferSize = 30;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte;
DMA_InitStructure.DMA_MemoryDataSize = DMA_PeripheralDataSize_Byte;
DMA_InitStructure.DMA_Mode = DMA_Mode_Normal;
DMA_InitStructure.DMA_Priority = DMA_Priority_VeryHigh;
DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;
DMA_Init(DMA1_Channel5, &DMA_InitStructure);
DMA_Cmd(DMA1_Channel5, ENABLE);
DMA_ITConfig(DMA1_Channel5,DMA_IT_TC | DMA_IT_TE,ENABLE);
}
void NVIC_Configuration(void)
{
NVIC_InitTypeDef NVIC_InitStructure;
NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 2;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
NVIC_InitStructure.NVIC_IRQChannel = DMA1_Channel4_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
NVIC_InitStructure.NVIC_IRQChannel = DMA1_Channel5_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
}
void USART1_IRQHandler(void)
{
uint8_t clear;
if(USART_GetITStatus(USART1,USART_IT_IDLE)!= RESET) // for USART_IT_IDLE
{
clear = USART1->SR; // clear IT_IDLE
clear = USART1->DR;
data_len = 30 - DMA_GetCurrDataCounter(DMA1_Channel5);
DMA_Cmd(DMA1_Channel5,DISABLE);
DMA_SetCurrDataCounter(DMA1_Channel5,30);
DMA_Cmd(DMA1_Channel5,ENABLE);
}
}
void DMA1_Channel4_IRQHandler(void)
{
if(DMA_GetITStatus(DMA1_FLAG_TC4) != RESET) // for DMA_IT_TC
{
DMA_ClearITPendingBit(DMA1_IT_TC4);
}
}
void DMA1_Channel5_IRQHandler(void)
{
if(DMA_GetITStatus(DMA1_IT_TC5) != RESET) // for DMA_IT_TC
{
DMA_ClearITPendingBit(DMA1_IT_TC5);
DMA_Cmd(DMA1_Channel5,DISABLE);
DMA_SetCurrDataCounter(DMA1_Channel5,30);
DMA_Cmd(DMA1_Channel5,ENABLE);
}
}
Solved! Go to Solution.
2021-10-14 6:18 PM
You can disable the idle interrupt flag at transmission complete if you don't want it to generate an interrupt later on.
USARTx->CR1 &= ~USART_CR1_IDLEIE;
2021-10-14 3:12 AM
2021-10-14 6:01 AM
> But the length of data is equal to 30 bytes, it enters the DMA1_Channel5_IRQHandler(void) function first then enters the USART1_IRQHandler(void) function again. Why does the length of data be equal to BufferSize cause Idle interruption?
The 30 bytes complete and the DMA TC interrupt fires, then at some later point the line becomes idle and the IDLE interrupt fires. What's unexpected about this?
2021-10-14 6:12 PM
I realize it becomes an idle and idle interrupt generator after the transmission is complete. How could I avoid idle interruptions to clear some register flag at TC point?
2021-10-14 6:18 PM
You can disable the idle interrupt flag at transmission complete if you don't want it to generate an interrupt later on.
USARTx->CR1 &= ~USART_CR1_IDLEIE;
2021-10-14 8:15 PM
Ok, this is a way without idle interrupt.
Thanks for your replies.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.