2015-10-29 1:00 AM
I'm having a big problem.
I have an USART which uses a circular buffer with DMA to receive characters.The machine sometimes has to save some informations in internal EEPROM.After some time, from minutes to many hours, the USART stops reception.Watching with emulator, it seems DMA is insensible, as freezed, but correctly set.The strange thing is that if I stop execution and then I continue, magically DMA resumes its operation...Obviously I can't do it without emulator.Is it possible that EEPROM writings could have some interference with DMA activity?For information, I used the standard peripheral library functions for EEPROM.Thanks in advanceWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.