2019-07-09 10:36 AM
Hello everyone,
so what I’m going to do is displaying the value of the temperature on the LCD of the STM32F413H-Disco with a PT100, i wrote this code:
int value;
char getvalue[20];
...
MX_ADC_Init();
HAL_ADC_Start_IT(&hadc1); (I choose Interruption because in reality i started with a simple potentiometer so I think that if I turn it faster I have to see the right value, I don’t want that the program run all the code and then display the value, that’s why I used the interruption )
HAL_ADC_PollForConversion(&hadc1, 100);
value = HAL_ADC_GetValue(&hadc1);
itoa(value, getvalue, 10);
..
GUI_Clear();
GUI_SetFont(....);
GUI_DisplayStringAt(...);
I declared the MX_ADC_Init function
but it displays 0 on the LCD.
Clive Two.Zero can you help me to resolve this please?
thanks
Solved! Go to Solution.
2019-07-10 11:29 AM
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.