2017-02-07 1:02 PM
Is a discovery board available for any of the stm32f417 variants?
#stm32f417 #stm32f4-discoverySolved! Go to Solution.
2017-02-07 1:34 PM
None I know of.
The only dedicated devboard I know of is the related
http://www.st.com/en/evaluation-tools/stm3241g-eval.html
, but it's a bit pricey, hundreds of $.In fact, I know of none of the DISCOs or NUCLEOs populated with any of the crypto-enabled STM32 variants.
The 'F417 is the same as 'F407, so as far as the peripherals are concerned, you can fully asses them with the '
.If you want to play specifically with the 'F417's crypto features, then one of the options is to buy either the 'F4 DISCO or any Nucleo144, plus a 'F417 in matching package, and swap it for what is on the board.
JW
2017-02-07 1:34 PM
None I know of.
The only dedicated devboard I know of is the related
http://www.st.com/en/evaluation-tools/stm3241g-eval.html
, but it's a bit pricey, hundreds of $.In fact, I know of none of the DISCOs or NUCLEOs populated with any of the crypto-enabled STM32 variants.
The 'F417 is the same as 'F407, so as far as the peripherals are concerned, you can fully asses them with the '
.If you want to play specifically with the 'F417's crypto features, then one of the options is to buy either the 'F4 DISCO or any Nucleo144, plus a 'F417 in matching package, and swap it for what is on the board.
JW
2017-02-07 2:29 PM
Mikroe has a number of boards with crypto chips.
https://shop.mikroe.com/development-boards/starter/clicker/stm32f4
Others have swapped parts on the DISCO, and I've populated my own boards with sample parts.
2017-02-07 2:47 PM
waclawek.jan wrote:
...If you want to play specifically with the 'F417's crypto features, then one of the options is to buy either the 'F4 DISCO or any Nucleo144, plus a 'F417 in matching package, and swap it for what is on the board.
JW
Absent the disco for the 417 this is what I'll do. Thanks!
2017-02-07 3:43 PM
Clive One wrote:
Mikroe has a number of boards with crypto chips.
/external-link.jspa?url=https%3A%2F%2Fshop.mikroe.com%2Fdevelopment-boards%2Fstarter%2Fclicker%2Fstm32f4
Others have swapped parts on the DISCO, and I've populated my own boards with sample parts.
Thank you for the vector. Mikroe has cool stuff! I wish I didn't need ethernet connectivity and crypto
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.