2013-02-19 6:50 PM
I have made baseboard PCBs for the Discovery-F4, Discovery-F3 and Discovery-VL that break out the signals to separate connectors for various ports and interfaces.
I am offering the PCBs for sale if you would find them helpful for a project.Photos, schematics, and BOM links are available on my blog:http://kornakprotoblog.blogspot.ca/2013/02/four-stm32-discovery-baseboards.html
Has anyone seen any other baseboards or expansion boards for the STM32 Discovery modules?1. I have links to the Embest STM32F4DIS-BB Ethernet baseboard for the Discovery-F4 on that page.2. Gage submitted a link (on Hackaday.com) to the wvshare.com Open-407-IC board which is very interesting. Search for Open407 on eBay, or take a look at this link:It does not use the Discovery-F4 module, but it comes with a similar module. #discovery-f4-stm32-f3-vl2013-02-19 7:41 PM
It does not use the Discovery-F4 module, but it comes with a similar module.
An arguably better board in fact, using the 176 pin LQFP instead of the 100 pin one, and not cluttered with other circuitry.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.