2023-05-02 6:03 AM
Hello,
we currently have a problem using PB6 of an STM32G474ME as FDCAN-TX: During Reset, it is pulled down to GND, which we attribute to the USB-C functionality. This causes the FDCAN-TX line to send a dominant signal during reset of the STM32.
As per p. 72 of the datasheet for the STM32G474xE (DS12288 Rev 6) the pull-down should be disabled by pulling PA9 low. However, we cannot reproduce this, even though we can disable the pull-down of PB4 via pulling PA10 low.
Is our understanding of the issue correct? Can be pull-down-resistor of PB6 be disabled via other means?
Greetings,
Bernd
2023-05-02 8:12 AM
Hello @BGott.1 and welcome to ST Community :smiling_face_with_smiling_eyes:,
In order to disable the pull down on PB6, you only need to set UCPD1_DBDIS bit in the PWR_CR3 register.
Hope that helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.