2007-11-04 9:09 PM
Development system hangs when DMA active
2011-05-17 3:17 AM
Hello
Perhaps this is not a Cortex only problem, but I try to post it here first. I use a STM32F103 (on a Keil board) my development system is IAR embedded workbench ver 4.42. I have an application that uses DMA to communicate on SPI. Most of the time everything is working fine, but sometimes (I suspect it is when I have shut down debugging while the DMA was active) I can not get in touch with the processor again. So when I try to flash the new SW, the system just hangs. The only solution I have found so far is to remove power from the board and plug it in again. Has anybody observed a similar problem, and come up with a more elegant solution?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.