2025-03-31 6:20 PM - edited 2025-03-31 6:22 PM
How does the bootloader in the STM32C071 system memory generate its 12-character USB serial number string descriptor (e.g. "205537C24236")? I notice some similarities between this serial number and the 96-bit unique device ID at address 0x1FFF7550, but overall they look very different. I'm asking because I would like my firmware to use the same serial number as the bootloader, and being able to use a compact serial number would be beneficial as well.
Here are some examples of the 96-bit unique ID (hex formatted, with dashes after every 2 bytes) and the corresponding 12-character USB serial number:
1: 7A00-2500-0150-3642-4837-3020, 205537C24236
2: 7B00-5700-0150-3642-4837-3020, 208737C34236
3: 7B00-2700-0150-3642-4837-3020, 205737C34236
4: 7B00-8100-0150-3642-4837-3020, 20B137C34236
I looked at the documentation of the unique ID in RM0490, section 30.1, but that documentation was partially incorrect and did not help.
Solved! Go to Solution.
2025-03-31 7:02 PM
I figured it out! I found a useful thread on this forum and it appears the STM32C0's bootloader is behaving the same was as the STM32F4, so you can generate the 16-bit words needed by doing:
uint16_t * const uid = (uint16_t *)UID_BASE;
uint16_t words[] = { uid[1] + uid[5], uid[0] + uid[4], uid[3] };
I would have just deleted my original post if I could find the option for that.
2025-03-31 7:02 PM
I figured it out! I found a useful thread on this forum and it appears the STM32C0's bootloader is behaving the same was as the STM32F4, so you can generate the 16-bit words needed by doing:
uint16_t * const uid = (uint16_t *)UID_BASE;
uint16_t words[] = { uid[1] + uid[5], uid[0] + uid[4], uid[3] };
I would have just deleted my original post if I could find the option for that.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.