2016-03-16 6:47 AM
Hello,
i'm using CubeMx 4.13 and I have this problem :Sometimes one file *.h generated by CubeMx is deleted when regenerating the project.In the Project settings in Code generator i use 'Generate peripherals initalization as a pair of '.c/.h' files per IP'.I have to regenerate the project to recreate the deleted file but all my user code included is lost.This problem happens at least once in ten and was already present in earlier version of CubeMx.Thanks.Philippe2016-03-16 7:19 AM
Hi Philippe,
Thank you for your feedback. The issue has been reported internally.-Syrine-2016-03-16 8:04 AM
Dear user,
We don't reproduce your issue. Also, can you please provide your .ioc file and indicate in which mode (standalone application, eclipse plug-in, command lines) and on which operating system you're running. Any specific .h file gets deleted? Thank you2016-03-18 7:53 AM
Hello,
here is my project. The main.c file is also rarely deleted. I use True Studio and my project is opened in True Studio when generating the project under CubeMx. The problem is very strange. Some days, no bug and some days it often happens . Thanks Philippe ________________ Attachments : ProjectBugDeleted_hFiles.ioc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzWX&d=%2Fa%2F0X0000000bN9%2FSpqZOKcKBB3zc5ulrxTdgr8lOmQZ7wVdUghO5ceaWNc&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.