2025-05-29 4:35 AM
I have a doubt about can a general purpose timer generate dead time like advanced timer without changing the duty and frequency is this is possible i tried with center aligned mode but it changes the duty is there is any possiblities??
2025-05-29 5:14 AM
what you can do is to, put a flag, when you want to start the "dead time", and in your timer routine, check for that flag, start counting the death time and then in the place where you said "start dead time", check for the "counting death time" to happen.
Hope it helps.
greetings
2025-05-29 5:54 AM
The general purpose timers do not have dead time functionality.
> without changing the duty and frequency
Any modification to the waveform will change one or the other. What exactly are you going for here?
2025-05-29 9:22 PM
I need the same functionality of advanced timer Pwm with dead time same requirements i want in general purpose timer that why i asked is there is any possibility
2025-05-29 9:23 PM
I didn't understand what you were exactly saying
2025-05-30 6:18 AM
No. The dead time feature on advanced timers is not available on general purpose timers.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.