2010-01-16 4:10 AM
DAC
2011-05-17 4:38 AM
Hi All,
I have just managed to get the on board DAC up and running with the assistance of the TwoChannels_TriangleWave standard peripheral example. I can see how to change the amplitude of the triangle wave by defining 'DAC_TriangleAmplitude_2047' etc... however I want to be able to change the amplitude (or the frequency) of the DAC output on the fly with a variable. Is this possible? FYI The plan is for the end device (with a filter etc...) to output a 4-20mA signal proportional to an RMS approximation of a recorded ADC buffer. Many Thanks, Paul.2011-05-17 4:38 AM
Paul,
You may want to consider using a timer (for example, in PWM mode) to create your current output. The pulse width and frequency of the timer can be easily modified ''on the fly''. Regards, ChrisWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.