2016-01-04 1:58 AM
I am using a STM32L152RE Nucleo Board and programming with EmBitz using the Standard Peripheral Library.
I am trying to generate a ramp signal using DAC channel 1 and DMA Channel 2 using Timer2 as trigger. The code does not work. However if I change to DAC channel 2, DMA channel 3 (changing DAC_DHR12R1_Address 0x40007408 to DAC_DHR12R2_Address 0x40007414) the code works. I really do not understand.Following is the code:#include ''stm32l1xx_conf.h''#include ''math.h''#define DAC_DHR12R1_Address 0x40007408#define WAVEPOINTS 200void GPIO_initialization(void);void DMA_DAC_initialize(void);void TIM2_initialize(void);uint16_t i;float j;uint16_t waveform[WAVEPOINTS];int main(void){ for(i = 0; i < WAVEPOINTS; i++) { waveform[i]= (uint16_t)(807 + 12*i); } GPIO_initialization(); DMA_DAC_initialize(); TIM2_initialize(); while(1) { }}void GPIO_initialization(void){ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); GPIO_InitTypeDef gpioStructure; gpioStructure.GPIO_Pin = GPIO_Pin_4; gpioStructure.GPIO_Mode = GPIO_Mode_AN; gpioStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; gpioStructure.GPIO_Speed = GPIO_Speed_2MHz; GPIO_Init(GPIOA, &gpioStructure);}void DMA_DAC_initialize(void){ RCC_APB1PeriphClockCmd(RCC_APB1Periph_DAC, ENABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE); DAC_InitTypeDef DAC_Structure; DAC_Structure.DAC_Trigger = DAC_Trigger_T2_TRGO; DAC_Structure.DAC_WaveGeneration = DAC_WaveGeneration_None; DAC_Structure.DAC_OutputBuffer = DAC_OutputBuffer_Enable; DAC_Init(DAC_Channel_1, &DAC_Structure); DMA_InitTypeDef DMA_Structure; DMA_DeInit(DMA1_Channel2); DMA_Structure.DMA_PeripheralBaseAddr = DAC_DHR12R1_Address; DMA_Structure.DMA_MemoryBaseAddr = (uint32_t) &waveform; DMA_Structure.DMA_DIR = DMA_DIR_PeripheralDST; DMA_Structure.DMA_BufferSize = WAVEPOINTS; DMA_Structure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_Structure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_Structure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; DMA_Structure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; DMA_Structure.DMA_Mode = DMA_Mode_Circular; DMA_Structure.DMA_Priority = DMA_Priority_High; DMA_Structure.DMA_M2M = DMA_M2M_Disable; DMA_Init(DMA1_Channel2, &DMA_Structure); DMA_Cmd(DMA1_Channel2, ENABLE); DAC_Init(DAC_Channel_1, &DAC_Structure); DAC_Cmd(DAC_Channel_1, ENABLE); DAC_DMACmd(DAC_Channel_1, ENABLE);}void TIM2_initialize(void){ // 100Hz sinewave -> period = 10ms, 200 samples each period -> DAC must be updated every 50 us RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); TIM_TimeBaseInitTypeDef timerInitStructure; timerInitStructure.TIM_Prescaler = 32-1; // frequency 1MHz -> 1us each step timerInitStructure.TIM_CounterMode = TIM_CounterMode_Up; timerInitStructure.TIM_Period = 50-1; timerInitStructure.TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseInit(TIM2, &timerInitStructure); TIM_SelectOutputTrigger(TIM2, TIM_TRGOSource_Update); TIM_Cmd(TIM2, ENABLE);}We’re moving the ST Community to a new platform to give you a better and more reliable community experience.