2017-03-15 1:58 AM
Hello,
I have programmed my board (STM32L475) with the example '...STMM32Cube_FW_L4_V1.7.0\Projects\STM32L476RG-Nucleo\Examples\PWR\PWR_STOP1_RTC\MDK-ARM'. I measure current consumption and it is higher than the expected one => it is about 80uA. Which is the reason of such high figure?
Best regards.
#stop1 #stm32l4 #current2017-03-15 2:28 AM
Hi
TARRAGO.DANIEL
,-Nesrine-
2017-03-15 8:50 AM
Hi,
It enters sleep mode. Furthermore I have noticed that there is no need for an external reset and I had one. I have removed this reset but now, in same situation (Stop1) current consumption has increased to around 230uA. I do not understand this situation!! And I have measured voltage at NRST pin: it is 1.87V and Vcc is 3.33V. Why do I get such difference?
Best regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.