2016-11-11 9:35 AM
For the STM32F0 device, in the standby mode after executing the function HAL_PWR_EnterSTANDBYMode(), will all the GPIO pins (except for the wakup pin and RTC tamper ...) are put in highZ mode? Or is it something I have to explicitly do in the codes?
Also, assuming all the GPIO pins are in highZ mode, based on the datasheet, the current consumption for the following are in worse case: Idd = 3.1uA Idda = 4.6uA RTC = 2.8uA Are these accurate? Are there any other source of current I should take into account? Thanks.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.