2021-06-16 1:11 AM
Hello,
I have a problem with my .HEX file generated with KEIL 5.
In STM32H753 there are two banks memory:
FIRST BANK MEMORY : 0x08000000-0x080FFFFF
SECOND BANK MEMORY : 0x08100000-0x081FFFFF
My project has this structure:
0x08000000-0x08060000=> My own Boot
0x08060000-0x081FFFFF => My own app
When I obtain .bin file of my project (it was been converted from .hex file) the file is always 1 Mb and it contains the code of FIRST BANK MEMORY.
How can I obtain both .hex file? from first and second bank memory?
thank you.
best regards.
Fabio
2021-06-17 6:24 AM
If you application fits within the first bank, it's not going to generate any code beyond that.
2021-06-17 6:38 AM
Unfortunatly, My app doesnt fit in First bank. It's large 0xc0000
2021-06-17 6:42 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.