2015-12-16 10:50 AM
Hi,
i m using stm32f103 nucleo board and keil compiler. I downloaded code from keil website for uart. and tried to compile the code but got error as some files are missing. following are the errors.C:\Keil_v5\ARM\PACK\Keil\STM32F1xx_DFP\1.1.0\Device\Include\stm32f10x_lib.h(32): error: #5: cannot open source input file ''stm32f10x_map.h'': No such file or directoryi have attached the downloaded code from keil side.2015-12-16 10:53 AM
here i have attached the code.
________________ Attachments : stm32_usart_irq.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1JL&d=%2Fa%2F0X0000000bl9%2FsztCWQzcUjMd87g62qKP.sU0nMMF5567SjCq9FTZUrc&asPdf=false2015-12-16 11:14 AM
Doesn't look to be code designed for uV5, it's far too old.
Have you loaded the legacy packs? Perhaps you can find some newer USART examples in that?2015-12-16 7:08 PM
Can you plz guide me with this.
i m new to stm32 controllers.2015-12-17 8:44 AM
Hi
I followed the following video to get compiler ready to work.https://www.youtube.com/watch?v=w9_8RVFBLIAthen also getting error as files are missing.i configure the keil as shown in video. and use the below code.[code]/************************* * stm32 uart main.c *************************/ #include ''stm32f10x.h'' /* User defined function prototypes */void GPIOA_Init(void);void USART1_Init(void);void led_toggle(void); int main(void){ /* Initialize GPIOA PIN8 */ GPIOA_Init(); /* Initialize USART1 */ USART1_Init(); while(1) { /* Do nothing, all happens in ISR */ }} /*********************************************** * Initialize GPIOA PIN8 as push-pull output ***********************************************/void GPIOA_Init(void){ /* Bit configuration structure for GPIOA PIN8 */ GPIO_InitTypeDef gpioa_init_struct = { GPIO_Pin_8, GPIO_Speed_50MHz, GPIO_Mode_Out_PP }; /* Enable PORT A clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE); /* Initialize GPIOA: 50MHz, PIN8, Push-pull Output */ GPIO_Init(GPIOA, &gpioa_init_struct); /* Turn off LED to start with */ GPIO_SetBits(GPIOA, GPIO_Pin_8);} /***************************************************** * Initialize USART1: enable interrupt on reception * of a character *****************************************************/void USART1_Init(void){ /* USART configuration structure for USART1 */ USART_InitTypeDef usart1_init_struct; /* Bit configuration structure for GPIOA PIN9 and PIN10 */ GPIO_InitTypeDef gpioa_init_struct; /* Enalbe clock for USART1, AFIO and GPIOA */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1 | RCC_APB2Periph_AFIO | RCC_APB2Periph_GPIOA, ENABLE); /* GPIOA PIN9 alternative function Tx */ gpioa_init_struct.GPIO_Pin = GPIO_Pin_9; gpioa_init_struct.GPIO_Speed = GPIO_Speed_50MHz; gpioa_init_struct.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOA, &gpioa_init_struct); /* GPIOA PIN9 alternative function Rx */ gpioa_init_struct.GPIO_Pin = GPIO_Pin_10; gpioa_init_struct.GPIO_Speed = GPIO_Speed_50MHz; gpioa_init_struct.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOA, &gpioa_init_struct); /* Enable USART1 */ USART_Cmd(USART1, ENABLE); /* Baud rate 9600, 8-bit data, One stop bit * No parity, Do both Rx and Tx, No HW flow control */ usart1_init_struct.USART_BaudRate = 9600; usart1_init_struct.USART_WordLength = USART_WordLength_8b; usart1_init_struct.USART_StopBits = USART_StopBits_1; usart1_init_struct.USART_Parity = USART_Parity_No ; usart1_init_struct.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; usart1_init_struct.USART_HardwareFlowControl = USART_HardwareFlowControl_None; /* Configure USART1 */ USART_Init(USART1, &usart1_init_struct); /* Enable RXNE interrupt */ USART_ITConfig(USART1, USART_IT_RXNE, ENABLE); /* Enable USART1 global interrupt */ NVIC_EnableIRQ(USART1_IRQn);} /******************************************* * Toggle LED *******************************************/void led_toggle(void){ /* Read LED output (GPIOA PIN8) status */ uint8_t led_bit = GPIO_ReadOutputDataBit(GPIOA, GPIO_Pin_8); /* If LED output set, clear it */ if(led_bit == (uint8_t)Bit_SET) { GPIO_ResetBits(GPIOA, GPIO_Pin_8); } /* If LED output clear, set it */ else { GPIO_SetBits(GPIOA, GPIO_Pin_8); }} /********************************************************** * USART1 interrupt request handler: on reception of a * character 't', toggle LED and transmit a character 'T' *********************************************************/void USART1_IRQHandler(void){ /* RXNE handler */ if(USART_GetITStatus(USART1, USART_IT_RXNE) != RESET) { /* If received 't', toggle LED and transmit 'T' */ if((char)USART_ReceiveData(USART1) == 't') { led_toggle(); USART_SendData(USART1, 'T'); /* Wait until Tx data register is empty, not really * required for this example but put in here anyway. */ /* while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET) { }*/ } } /* ------------------------------------------------------------ */ /* Other USART1 interrupts handler can go here ... */} [/code]Plz help me with this.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.