2015-09-14 10:15 PM
I have a minimum STM32F103ZET6 system board with. I have downloaded STM32CubeF1(Version 1.2.0) package. I build a simple project, which just blink a led, and I compile it with no error/warning. The main.c source code is shown below
#include''stm32f1xx_hal.h''#include''stm32f1xx_hal_gpio.h''#include''stm32f1xx_hal_rcc.h''#include''stm32f1xx_hal_rcc_ex.h''#include''stdint.h''void m_delay(volatile uint32_t m_time){ while(m_time > 0){ m_time--; }}void SystemClock_Config(){ RCC_ClkInitTypeDef Clk_InitStructure = {0}; RCC_OscInitTypeDef Osc_InitStructure = {0}; Osc_InitStructure.OscillatorType = RCC_OSCILLATORTYPE_HSE; Osc_InitStructure.HSEState = RCC_HSE_ON; Osc_InitStructure.HSEPredivValue = RCC_HSE_PREDIV_DIV1; Osc_InitStructure.PLL.PLLState = RCC_PLL_ON; */ Osc_InitStructure.PLL.PLLSource = RCC_PLLSOURCE_HSE; Osc_InitStructure.PLL.PLLMUL = RCC_PLL_MUL9; if (HAL_RCC_OscConfig(&Osc_InitStructure)!= HAL_OK) { /* Initialization Error */ while(1); } /* Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2 clocks dividers */ Clk_InitStructure.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2); Clk_InitStructure.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; Clk_InitStructure.AHBCLKDivider = RCC_SYSCLK_DIV1; Clk_InitStructure.APB2CLKDivider = RCC_HCLK_DIV1; Clk_InitStructure.APB1CLKDivider = RCC_HCLK_DIV2; if (HAL_RCC_ClockConfig(&Clk_InitStructure, FLASH_LATENCY_2)!= HAL_OK) { /* Initialization Error */ while(1); }}int main(){ HAL_Init(); SystemClock_Config(); __HAL_RCC_GPIOG_CLK_ENABLE(); GPIO_InitTypeDef GPIO_InitStructure; GPIO_InitStructure.Pin = GPIO_PIN_14; GPIO_InitStructure.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStructure.Pull = GPIO_PULLUP; GPIO_InitStructure.Speed = GPIO_SPEED_HIGH; HAL_GPIO_Init(GPIOG, &GPIO_InitStructure); while(1){ HAL_GPIO_WritePin(GPIOG, GPIO_PIN_14, 1); HAL_Delay(500); HAL_GPIO_WritePin(GPIOG, GPIO_PIN_14, 0); HAL_Delay(500); } return 0;}But it didn't work well. The pin output HIGH and didn't change its value. It looks like the program block at ''HAL_GPIO_WritePin(GPIOG, GPIO_PIN_14, 1)''. Even I change the HAL_Delay() to the function I write m_delay(), it also can be blocked. So what wrong with my code?2015-09-15 3:26 AM
Hi yuzhou.huang,
I suggest you:1- Debug your code as the problem may be caused by clock configuration code for example, not GPIO related function2- Have a look to the example STM32Cube_FW_F1_V1.2.0\Projects\STM32F103RB-Nucleo\Examples\GPIO\GPIO_IOToggle implementing similar functionality as what you want.3- Use the STM32CubeMX tool to generate initialization project to which you may add your own code.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-09-15 6:04 AM
If the external clocks, or internal PLL, don't start correctly you're going to fall into one of the while(1) tar pits. Add code to identify where it's stuck, output via a GPIO/LED or USART.
2015-09-16 8:27 AM
Hello,
HAL_Delay(500); requires SysTick_Handler() did you implement it? Otherwise the tick counter doesn't increment and you are stall in HAL_Delay().void SysTick_Handler(void)
{
HAL_IncTick();
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.