2018-01-16 4:03 AM
Hi ,
I am generating usart2 in STM43F407 Discovery using stmcubemx and keil where it does not work and the configuration in stmcube is as follows : > rcc - crystal oscillator - HSEPLL Source > USART2 - asynchronous -9600baud- 8bit data Data should be 'Hello World\n' it appears on the terminal corrupted data/* Includes ------------------------------------------------------------------*/
#include 'main.h' #include 'stm32f4xx_hal.h' #include <string.h> UART_HandleTypeDef huart2; char test[]='Hello World\n';void SystemClock_Config(void);
static void MX_GPIO_Init(void); static void MX_USART2_UART_Init(void);int main(void)
{ HAL_Init(); SystemClock_Config(); MX_GPIO_Init(); MX_USART2_UART_Init(); while (1) { HAL_UART_Transmit(&huart2,(uint8_t *)test,strlen(test),100); HAL_Delay(1000);}
}
void SystemClock_Config(void) {RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;/**Configure the main internal regulator output voltage
*/ __HAL_RCC_PWR_CLK_ENABLE();__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/**Initializes the CPU, AHB and APB busses clocks
*/ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLM = 25; RCC_OscInitStruct.PLL.PLLN = 168; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLQ = 4; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }/**Initializes the CPU, AHB and APB busses clocks
*/ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{ _Error_Handler(__FILE__, __LINE__); }/**Configure the Systick interrupt time
*/ HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);/**Configure the Systick
*/ HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0); }/* USART2 init function */
static void MX_USART2_UART_Init(void) {huart2.Instance = USART2;
huart2.Init.BaudRate = 9600; huart2.Init.WordLength = UART_WORDLENGTH_8B; huart2.Init.StopBits = UART_STOPBITS_1; huart2.Init.Parity = UART_PARITY_NONE; huart2.Init.Mode = UART_MODE_TX_RX; huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart2.Init.OverSampling = UART_OVERSAMPLING_16; if (HAL_UART_Init(&huart2) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }}
/** Configure pins as
* Analog * Input * Output * EVENT_OUT * EXTI */ static void MX_GPIO_Init(void) {/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOH_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE();}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence. * @param None * @retval None */ void _Error_Handler(char * file, int line) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ while(1) { } /* USER CODE END Error_Handler_Debug */ }#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t* file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf('Wrong parameters value: file %s on line %d\r\n', file, line) */ /* USER CODE END 6 */}
#endif
/**
* @} *//**
* @} */ Note: this post was migrated and contained many threaded conversations, some content may be missing.2018-01-16 6:24 AM
>baud =9600, data bits=8 , stop bits =1.
> STM32F407VG connected to UART TTL to USB CONVERTER and I tested this TTL TO USB converter with different modules while it is working fine.
2018-01-16 6:31 AM
When you say, 'TTL' - it is for 3V, isn't it?
And you do have a good ground connection, don't you?
2018-01-16 6:41 AM
> TTL connected for 3.3 v not 5v and powered from pc usb
> STM32F4 Discovery also powered from pc usb
connection from it is tested using GSM Sim808 and the same terminal sending AT Commands and it worked successfuly
2018-01-16 6:45 AM
Do you have any logic analyser to sniff the UART? This way we can eliminate wiring errors (right pins), etc
2018-01-16 6:51 AM
No
2018-01-16 6:56 AM
Before I bought the logic analyser I usually sampled the output through the ADC (poor man scope) to see the timing.
2018-01-16 8:09 AM
I generated the project for STM32F401-Disco (do not have F407) using HSI/PLL and UART2/115200 worked fine.
2018-01-16 8:47 AM
The STM32F407-DISCO has an 8 MHz HSE clock input, this must be selected via the PLL and also the HSE_VALUE define
2018-01-16 10:04 AM
I tested it and worked using your advice so , I need to thank you for your great help .
Turvey.Clive.002
2018-01-16 10:06 AM
Thanks Mr
Golab.Bogdan
I solved it , where it was my mistake as I set HSE (High speed external clock) as either 25 or 16 MHZ as it should be 8MHZ , So your advices regarding uart helped me and gave me great ideas and for sure I got great knowledge from our conversation.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.