2008-07-22 5:44 AM
Conversion of more regular channels using DMA
2011-05-17 3:40 AM
I'm trying to converte 2 regular ADC channels, but it does not worke. I'm using DMA to put the result in memory.
Every time an adc-conversion is over, a DMA request should be generated, and the data moved to a buffer in memory. But when I check the buffer, it only contains results from the first channel in the ADC-queue. The length of the ADC-queue is set to 2, and the DMA seems to work correctly. The problem must be that the ADC don´t convert the next channel in the queue or the ADC don't generate a DMA request after end of conversion of the second channel in the queue. Any ideas how to get this to work?2011-05-17 3:40 AM
it should be something like this
DMA_InitStructure.DMA_PeripheralBaseAddr = ADC1_DR_Address; DMA_InitStructure.DMA_MemoryBaseAddr = (u32)ADC_RegularConvertedValueTab; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC; DMA_InitStructure.DMA_BufferSize =16; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_M2M = DMA_M2M_Disable; DMA_Init(DMA_Channel1, &DMA_InitStructure);We’re moving the ST Community to a new platform to give you a better and more reliable community experience.