2020-03-03 5:28 AM
Hello everybody,
I use the STM32H743 and try to flash it via UART, which usually works quite well.
I would like to know whether it is important to de-energize the controller before connecting the programming adapter or the adapter must be connected under voltage?
Here is the error that I encountered after some time:
when trying to start the bootloader, the reset pin was permanently set to low, so that the controller is in a permanent reset. The controller does not run the last flashed program, nor can I start communication with the bootloader.
I thank you in advance for the help!
2020-03-03 6:30 AM
Check the voltages on the supply and VCAP pins in this condition.
Especially VDDA
Check any BOM or PDR options or pin configurations.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.