2010-09-01 6:51 AM
Connecting to TMS320 Host Port Interface via FSMC
2011-05-17 5:05 AM
I would also love to know the asnwer. Did you found out anything?
I need to interface 8 bit SRAM with FSMC. It's address bus is connected through latches, so I need multiplexed access (like NOR memory type). But in ref-man, this combination is not stated in table NOR Flash/PSRAM supported memories and transactions. Everything have 16 bit memory data size :-(. Is there any possibility to use this type of SRAM connection? MCU: STM32F103VET6 SRAM: R1LV0408CSA Signals on SRAM: A[00-15] multiplexed A[16-18] direct D[0-7] direct CS, OE, WE direct Thanks, ViktorWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.