2019-12-08 1:35 PM
Currently I am trying to configure a second interrupt pin using CMSIS.
SYSCFG->EXTICR[1] = (SYSCFG->EXTICR[1] & ~SYSCFG_EXTICR2_EXTI6)|(0b0000 << SYSCFG_EXTICR2_EXTI6_Pos);
EXTI->FTSR = EXTI_FTSR_TR6;
EXTI->RTSR = EXTI_RTSR_TR6;
EXTI->IMR = EXTI_IMR_MR6;
NVIC_EnableIRQ(EXTI9_5_IRQn);
with void EXTI9_5_IRQHandler(void){} works.
But when I try to add another button for interrupt;
SYSCFG->EXTICR[0] = (SYSCFG->EXTICR[0] & ~SYSCFG_EXTICR1_EXTI3)|(0b0000 << SYSCFG_EXTICR1_EXTI3_Pos);
EXTI->FTSR = EXTI_FTSR_TR3;
EXTI->RTSR = EXTI_RTSR_TR3;
EXTI->IMR = EXTI_IMR_MR3;
NVIC_EnableIRQ(EXTI3_IRQn);
with void EXTI3_IRQHandler(void){}.
It doesn't do anything...
Why is it that the one above does work and the second one doesn't?
2019-12-08 2:08 PM
PA6 and PA3?
Which STM32 model? A "known good" board such as Nucleo/Disco, or something else?
Is PA3 properly connected? Can you see the input level change in respective bit of GPIOA_IDR? Isn't this pin set as Analog in GPIO?
Check in disasm, if the IRQ handler is properly inserted into the vector table.
JW
PS. Change your username to a normal nick.
2019-12-08 2:29 PM
Yes, it is PA6 and PA3.
Model is Nucleo F303RE. I guess it really is a software related issue..
GPIOA->MODER = (GPIOA->MODER & ~GPIO_MODER_MODER3)|(0b00 << GPIO_MODER_MODER3_Pos);
GPIOA->PUPDR = (GPIOA->PUPDR & ~GPIO_PUPDR_PUPDR3)|(0b10 << GPIO_PUPDR_PUPDR3_Pos);
When pushing the button, the interrupt isn't even called
2019-12-08 2:50 PM
Can you see the level changes in IDR?
Is the ISR address inserted in the vector table?
JW
2019-12-08 2:54 PM
I think I can test the first one with a seperate program where I toggle a LED.
Not so sure how to test the second question?
2019-12-08 2:57 PM
On Nuclea64, PA3 is connected to STLink's virtual-comm Tx. See the Nucleo's UM1724. Disconnect SB14.
JW
2019-12-09 2:26 AM
Didn't know how to disconnect SB14.
I tried changing everything to PC01, still doesn't work.
When I write a program to turn on / off a LED it works fine, so the pin itself is configured right.
The problem lays in the configuration of the interrupt.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.