2013-06-21 2:13 AM
Page 164 of RM0033 shows that EXTI0 can be used for Px[0], EXTI1-Px[1]... and so on only.
That means if I used PA0 pin as interrupt somewhere then I can used PB0, PC0... pins as interrupt source any more???2013-06-25 9:46 AM
Yes it is the case.
Only 16 interrupts can be simultaneously used when the EXTI lines are connected to GPIO pins. In fact, an interrupt cannot be configured in PA1 & another one in PB1 for example at the same time. -Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.