2017-12-23 10:02 PM
Hi everybody!
I am working on a design using STM32F407VGT6 runs at 168MHz, I want to enable an external line interrupt with rising signal edge. I am monitoring a signal from some system which when reachs 1.3V I should consider this as high voltage and execute its ISR. After some testing I see that when MCU input signal reach 1.5v and avove(up to 3v my VDD supply voltage) it considers it as high so is there any way I can decrease this minimum active high voltage to 1.3v so I can connect to the system directly without using comparator OP-AMP and once signal reach 1.3v, MCU considers it as rising edge and execute the ISR. Is it good to decrease the system VDD to 2.6v or it will affect something else like the clock I am working on.
Thanks
2017-12-24 2:01 AM
How about ADC Analog Watchdog function? When the trigger voltage has to be precise, it's an analog function.
2017-12-24 5:10 AM
For digital inputs, the logic levels are fixed by the hardware, and defined in the datasheet.
What you describe is making an analogue voltage measurement, and taking a decision based on the analogue result - so, as already noted, you will need to use an ADC.
2017-12-24 12:22 PM
https://learn.sparkfun.com/tutorials/logic-levels/33-v-cmos-logic-levels
How about lowering your power supply voltage? Power supply voltage and logic levels are related, so if you can use something close to 1.3v it might work. But not at 168MHz probably.
2017-12-25 1:35 PM
electronically, there are 2 diode drops to trigger the switching. is about 1.1-1.3V (basically TTL)
but the tolerance is loose, it will trigger 100% approx >= 1.0V & < 1.4V
Although the pin input schmitt trigger does work.(100-200mV), a comparator and a DAC would do a tighter job.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.