2014-07-17 11:39 PM
Hi,
I'm using the device STM32F030C8T6 that has all the timers count at 16-bit. I need using the timer count at 32-bit. In the data sheet in the page 67 reads ''Maximum possible count with 32-bit counter''. How can I configure the timer to count up to 32-bit? Thanks2014-07-18 6:19 AM
Some STM32F0 parts have a 32-bit counter, the part you have chosen does not.
You'd need to cascade at pair of 16-bit counters in master/slave mode This might be illustrative STM32F10x_StdPeriph_Lib_V3.5.0\Project\STM32F10x_StdPeriph_Examples\TIM\Cascade_Synchro2014-07-18 7:22 AM
Ok, Thanks
2014-07-21 12:44 AM
I have configurated the TIM2 and TIM3 in cascade mode:
uint8_t TIMER_ConfigSynchInCascade( void ) { TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_OCInitTypeDef TIM_OCInitStructure; /* TIM2 and TIM3 clock enable */ // -------------------------------------------------------------------------- RCC_APB2PeriphClockCmd(RCC_APB1Periph_TIM2 | RCC_APB1Periph_TIM3, ENABLE); /* Time base configuration */ // -------------------------------------------------------------------------- TIM_TimeBaseStructure.TIM_Period = 65535; TIM_TimeBaseStructure.TIM_Prescaler = 15; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure); TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure); /* Select the Master Slave Mode */ TIM_SelectMasterSlaveMode(TIM2, TIM_MasterSlaveMode_Enable); /* Master Mode selection */ TIM_SelectOutputTrigger(TIM2, TIM_TRGOSource_Update); /* Slave Mode selection: TIM3 */ TIM_SelectSlaveMode(TIM3, TIM_SlaveMode_Gated); TIM_SelectInputTrigger(TIM3, TIM_TS_ITR1); /* TIM enable counter */ TIM_Cmd(TIM3, ENABLE); TIM_Cmd(TIM2, ENABLE); return 0; } In the main function
, the LED4is
turned on and off
in the following mode:
static __IO uint8_t Debug = 0; #define LEDToggleValue ((uint32_t) 100000) static __IO uint32_t CounterTimers = 0; int main(void) { /* Initialize Leds mounted on STM3210X-EVAL board */ STM_EVAL_LEDInit(LED4); // Configura i timers in cascata TIMER_ConfigSynchInCascade(); while (1) { // Toggle led CounterTimers = TIMER_GetCounter(TIM2)+TIMER_GetCounter(TIM3); if ( CounterTimers > LEDToggleValue ) STM_EVAL_LEDOn(LED4); else STM_EVAL_LEDOff(LED4); } } The LED4 is ever off!I have
done something wrong
in the configuration
? Thanks2014-07-21 7:11 AM
Hi,
Not sure but I think you should use :RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2 | RCC_APB1Periph_TIM3, ENABLE); instead of RCC_APB2PeriphClockCmd(RCC_APB1Periph_TIM2 | RCC_APB1Periph_TIM3, ENABLE);2014-07-21 8:34 AM
CounterTimers = TIMER_GetCounter(TIM2)+TIMER_GetCounter(TIM3);
Does these functions deal with shifting the 16-bit word suitably?2014-07-21 11:45 PM
I have corrected the errors, but the timer TIM3 not counter!
The TIMER_GetCounter(TIM2) function return the value in the range [0÷65535], but the TIMER_GetCounter(TIM3) function return zero.2014-07-23 11:38 PM
The solution is descript below:
uint8_t TIMER_ConfigSynchInCascade( void ) { TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; uint16_t PrescalerValue_RPM = 0; RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM16 | RCC_APB2Periph_TIM17, ENABLE); /* Timer frequency configuration at 12 MHz */ PrescalerValue_RPM = (uint16_t) (SystemCoreClock / 12000000) - 1; /* Time base configuration */ TIM_TimeBaseStructure.TIM_Period = 65535; TIM_TimeBaseStructure.TIM_Prescaler = PrescalerValue_RPM; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM16, &TIM_TimeBaseStructure); TIM_TimeBaseInit(TIM17, &TIM_TimeBaseStructure); /* Select the Master Slave Mode */ TIM_SelectMasterSlaveMode(TIM16, TIM_MasterSlaveMode_Enable); /* Master Mode selection */ TIM_SelectOutputTrigger(TIM16, TIM_TRGOSource_Update); /* Slave Mode selection: TIM17 */ TIM_SelectSlaveMode(TIM17, TIM_SlaveMode_Gated); TIM_SelectInputTrigger(TIM17, TIM_TS_ITR1); /* Select the Master Slave Mode */ TIM_SelectMasterSlaveMode(TIM17, TIM_MasterSlaveMode_Enable); /* Master Mode selection: TIM17 */ TIM_SelectOutputTrigger(TIM17, TIM_TRGOSource_Update); /* TIM enable counter */ TIM_Cmd(TIM17, ENABLE); TIM_Cmd(TIM16, ENABLE); return 0; } The function that return the counter value at 32-bit is: uint32_t GetCounter32Bit ( void ) { uint16_t a, b, c, d; /* Reading twice to avoid overflow in the middle of reading */ a = TIM16->CNT; b = TIM17->CNT; c = TIM16->CNT; d = TIM17->CNT; if((a != c) || (b != d)) return ((uint32_t)c << 16) | d; else return ((uint32_t)a << 16) | b; }I
hope this is
clear
!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.