2017-12-30 8:56 AM
Hello,
I try to make my first baybesteps in arm cortex M. I use the free version of uVision 5. Currently I try to set up an USART. When I try to compile, I get the both erros below about 2*30 times out of stm32l4xx_ll_usart.h and stm32l4xx_ll_rcc.h:
_STATIC_INLINE void LL_USART_EnableDirectionTx(USART_TypeDef *
SARTx)_SRC\../_HDR/../_HDR/stm32l4xx_ll_usart.h(649): error: #90: function returning function is not allowed _STATIC_INLINE void LL_USART_EnableDirectionTx(USART_TypeDef *SARTx)_SRC\../_HDR/../_HDR/stm32l4xx_ll_usart.h(649): error: #141-D: unnamed prototyped parameters not allowed when body is present __STATIC_INLINE void LL_USART_EnableDirectionTx(USART_TypeDef *USARTx)_SRC\../_HDR/../_HDR/stm32l4xx_ll_usart.h(660): error: #79: expected a type specifierI try to compile one usart example without any erros. So I checked and copied the project settings. but without any new result. Still errors.
Does someone has any idea which helps me to fix my mistake?
Kind regards
Solved! Go to Solution.
2018-01-04 4:23 AM
I don't know, what I have done (maybe cleaning the project, delete the files and add it new to the project). But the errors are gone now... Don't know ..
2018-01-04 4:23 AM
I don't know, what I have done (maybe cleaning the project, delete the files and add it new to the project). But the errors are gone now... Don't know ..
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.