2008-03-13 1:12 AM
compilation issue
2011-05-17 3:26 AM
Hi,
i use codesourcery g++ lite. i used ld - T generic.hosted.ld stm32.ld i got main.bin file size more in MBs.I want use sprintf ,printf function. what is the procedure to do ld? following files size: Volume in drive D is Data Volume Serial Number is 681B-B60B Directory of D:\nagendra\Example7 03/13/2008 10:38 AM . 03/13/2008 10:38 AM .. 03/13/2008 10:12 AM lib 03/13/2008 10:36 AM 402,653,192 main.bin 03/13/2008 10:15 AM 8,885 main.c 03/13/2008 10:36 AM 152,026 main.elf 03/13/2008 10:36 AM 103,545 main.elf.map 10/08/2007 12:50 AM 2,580 main.h 03/13/2008 10:36 AM 6,128 main.o 03/13/2008 10:36 AM 1,915 makefile 03/13/2008 10:37 AM 104 nagen 10/08/2007 12:50 AM 2,759 readme.txt 02/01/2008 12:18 AM 973 stm32.ld 10/08/2007 12:50 AM 5,570 stm32f10x_conf.h 10/08/2007 12:50 AM 22,695 stm32f10x_it.c 10/08/2007 12:50 AM 3,267 stm32f10x_it.h 03/13/2008 10:36 AM 13,128 stm32f10x_it.o 03/13/2008 10:38 AM 0 test.txt 15 File(s) 402,976,767 bytes 3 Dir(s) 19,790,196,736 bytes free is there any solution to resolve size ? regards nagendra2011-05-17 3:26 AM
where did you get the linker scripts from?
2011-05-17 3:26 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.