2018-01-19 1:34 AM
Hello i have any question about Comp in STM32F3
1. W
hat is the p
ropagation delay for low overdrive, for example 5mV? In DS is only for 100mV. For High speed mode.2. W
hat is the output current for Low and high level on output commparatar?
3. What is the large-signal differential voltage amplification?
4. If is used internal DAC for driving one comparator input, can be used DAC without buffer?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.