2018-08-20 11:06 AM
Hi there, dumb, dumb, dumb, dumb question: which of the above, as reported by my Keil MDK compiler, count against my program space and which count against my RAM? Does CODE+RO go into my program space, or just CODE?
Asking because I'm playing with techniques to get image data into my program, and found an example project that does this:
static const uint8_t pixelmap_ButtonVideo[] =
{
/*Pixel format: Alpha 8 bit, Red: 8 bit, Green: 8 bit, Blue: 8 bit*/
0x00, 0x00, 0x00, 0x00
...
}and the static const ends up going into my RO tally, and I'm embarrassed to say I'm not 100% sure where that goes.
Thanks very much!
2018-08-20 11:16 AM
RO data stays in FLASH (see .MAP addresses, between 0x08000000..0x081FFFFF, or whatever)
RW is initialized data which stages in FLASH and gets copied/unpacked to RAM via __main/scatterload
ZI is zero initialized memory, it is described in a load region table with the RW data, and cleared by __main/scatterload
2018-08-20 12:08 PM
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.