2015-06-23 11:39 AM
Hello
I tried to compile and run arm_fft_bin_example of the cmsis package but there is a problem.
The problem is in the arm_bitreversal2.s file that can't be compiled by keil.
Is there any workaround and solution?
Thanks.
2015-06-23 12:01 PM
Yes, there is.
2015-06-23 12:06 PM
Hello
Here is the modified and working code for cortex-m4:
AREA ||.text||, CODE, READONLY, ALIGN=2
THUMB
;
/*
;* @brief In-place bit reversal function.
;* @param[in, out] *pSrc points to the in-place buffer of unknown 32-bit data type.
;* @param[in] bitRevLen bit reversal table length
;* @param[in] *pBitRevTab points to bit reversal table.
;* @return none.
;*/
EXPORT arm_bitreversal_32
EXPORT arm_bitreversal_16
arm_bitreversal_32 PROC
ADDS r3,r1,#1
CMP r3,#1
IT LS
BXLS lr
PUSH {r4-r9}
ADDS r1,r2,#2
LSRS r3,r3,#2
arm_bitreversal_32_0 ;
/* loop unrolled by 2 */
LDRH r8,[r1,#4]
LDRH r9,[r1,#2]
LDRH r2,[r1,#0]
LDRH r12,[r1,#-2]
ADD r8,r0,r8
ADD r9,r0,r9
ADD r2,r0,r2
ADD r12,r0,r12
LDR r7,[r9,#0]
LDR r6,[r8,#0]
LDR r5,[r2,#0]
LDR r4,[r12,#0]
STR r6,[r9,#0]
STR r7,[r8,#0]
STR r5,[r12,#0]
STR r4,[r2,#0]
LDR r7,[r9,#4]
LDR r6,[r8,#4]
LDR r5,[r2,#4]
LDR r4,[r12,#4]
STR r6,[r9,#4]
STR r7,[r8,#4]
STR r5,[r12,#4]
STR r4,[r2,#4]
ADDS r1,r1,#8
SUBS r3,r3,#1
BNE arm_bitreversal_32_0
POP {r4-r9}
BX lr
ENDP
arm_bitreversal_16 PROC
ADDS r3,r1,#1
CMP r3,#1
IT LS
BXLS lr
PUSH {r4-r9}
ADDS r1,r2,#2
LSRS r3,r3,#2
arm_bitreversal_16_0 ;
/* loop unrolled by 2 */
LDRH r8,[r1,#4]
LDRH r9,[r1,#2]
LDRH r2,[r1,#0]
LDRH r12,[r1,#-2]
ADD r8,r0,r8,LSR #1
ADD r9,r0,r9,LSR #1
ADD r2,r0,r2,LSR #1
ADD r12,r0,r12,LSR #1
LDR r7,[r9,#0]
LDR r6,[r8,#0]
LDR r5,[r2,#0]
LDR r4,[r12,#0]
STR r6,[r9,#0]
STR r7,[r8,#0]
STR r5,[r12,#0]
STR r4,[r2,#0]
ADDS r1,r1,#8
SUBS r3,r3,#1
BNE arm_bitreversal_16_0
POP {r4-r9}
BX lr
ENDP
END
2015-06-24 1:10 AM
by defining the following expression in the
options for target->
Asm->
Misc Controls, problem will be solved.
--cpreproc
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.