2010-07-12 2:31 AM
Clock setup problem
2011-05-17 4:58 AM
Hi Alex,
Just before I try this on my board, sorry to ask a daft question but do you have STM32F10X_CL defined? Martin.2011-05-17 4:58 AM
You might need to recompile FWLib... at least it was necessary on some older versions when changing HSE_Value.
2011-05-17 4:58 AM
Hello,
Thanks for those answers, STM32F10X_CL is defined as well as USE_STDPERIPH_DRIVER.
I've tried to recompile the entire project and still have the same problem ....Alex2011-05-17 4:58 AM
I found the problem!
When using PREDIV1 as a divider by 2 you have to write in two different registers (CFGR and CFGR2).
I've basicaly replaced RCC_CFGR_PLLXTPRE_PREDIV1by RCC_CFGR_PLLXTPRE_PREDIV1_Div2 (RM0008 Rev 11 page 144 explains why)
[code]
#ifdef STM32F10X_CL
/* Configure PLLs ------------------------------------------------------*/
/* PLL2 configuration: PLL2CLK = (HSE / 4) * 8 = 32 MHz */
/* PREDIV1 configuration: PREDIV1CLK = HSE / 2 = 8 MHz */
RCC->CFGR2 &= (uint32_t)~(RCC_CFGR2_PREDIV2 | RCC_CFGR2_PLL2MUL |
RCC_CFGR2_PREDIV1 | RCC_CFGR2_PREDIV1SRC);
RCC->CFGR2 |= (uint32_t)(RCC_CFGR2_PREDIV2_DIV2 | RCC_CFGR2_PLL2MUL8 |
RCC_CFGR2_PREDIV1SRC_HSE | RCC_CFGR2_PREDIV1_DIV2);
/* Enable PLL2 */
RCC->CR |= RCC_CR_PLL2ON;
/* Wait till PLL2 is ready */
while((RCC->CR & RCC_CR_PLL2RDY) == 0)
{
}
/* PLL configuration: PLLCLK = PREDIV1 * 9 = 72 MHz */
RCC->CFGR &= (uint32_t)~(RCC_CFGR_PLLXTPRE | RCC_CFGR_PLLSRC | RCC_CFGR_PLLMULL);
RCC->CFGR |= (uint32_t)(RCC_CFGR_PLLXTPRE_PREDIV1_Div2 | RCC_CFGR_PLLSRC_PREDIV1 |
RCC_CFGR_PLLMULL9);
#else
[/code]Alex
2011-05-17 4:58 AM
Hi Alex,
Cool. Keil simulator was showing HCLK @ 144MHz. I personally prefer using the ST library calls and setting up manually like on the 103. Cheers, Martin.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.