2015-03-06 1:52 AM
I am using a STM32F303 and need a very high stability clock ie around 1ppm over temperature. One of the modules I am looking at outputs what is described as ''clipped sine''. Can this drive the oscillator input on the MCU without problems?
#clock #stm32f3032015-03-06 7:51 AM
clipped sine = square wave with a crappy slew rate.
Provided it meets the VIL/VIH requirements I expect it to work fine.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.