2015-09-14 11:00 AM
Hi,
I'm using a servo with a pwm connection and this is a part of code:RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource4, GPIO_AF_1);
GPIO_InitTypeDef GPIO_InitStructure;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOB, &GPIO_InitStructure);
TIM_TimeBaseInitTypeDef TIM_BaseStruct;
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);
TIM_BaseStruct.TIM_Prescaler = 48-1;
TIM_BaseStruct.TIM_CounterMode = TIM_CounterMode_Up;
TIM_BaseStruct.TIM_Period = 20000-1;
TIM_BaseStruct.TIM_ClockDivision = TIM_CKD_DIV1;
TIM_BaseStruct.TIM_RepetitionCounter = 0;
TIM_TimeBaseInit(TIM3, &TIM_BaseStruct);
TIM_Cmd(TIM3, ENABLE);
TIM_OCInitTypeDef TIM_OCStruct;
TIM_OCStruct.TIM_OCMode = TIM_OCMode_PWM2;
TIM_OCStruct.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCStruct.TIM_OCPolarity = TIM_OCPolarity_Low;
/* 50% duty cycle */
TIM_OCStruct.TIM_Pulse = 10000;
TIM_OC1Init(TIM3, &TIM_OCStruct);
TIM_OC1PreloadConfig(TIM3, TIM_OCPreload_Enable); How can I change dinamically TIM_Pulse? (I'm using ST32F0xx)
2015-09-14 12:05 PM
TIM3->CCR1 = width in micro seconds, or TIM_SetCompare1(TIM3, x);
So perhaps a value between 600 to 2400, or 1500 top-centre, for a servoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.