2015-04-24 6:14 AM
The problem is simple. I uploaded a buggy program using ST-Link to a stm32f303 prototype board. The bug was that the routine that kicks the watchdog in the power supervisor does not work. Therefore it keeps resetting the MCU. While this is happening I cannot connect using ST-Link in any mode. Anything I'm missing or is it soldering time?
2015-04-24 6:26 AM
Pull BOOT0 High
Or try other ''connect under reset'' ''hold in reset'' type options2015-04-24 6:39 AM
BOOT0 is tied low at present, and I have tried all the ST-Link options. I think it doesn't like the reset line flipping up and down while it is trying to connect. I'll probably just do the capacitor to GND on the NRST reset line
2015-04-24 8:01 AM
And if you pull it into a high state at reset it will stop running your buggy code and you'll be able to erase it, and start over...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.