cancel
Showing results for 
Search instead for 
Did you mean: 

Case enable DCache (SCB_EnableDCache ()), camera image breaking phenomenon

togsin
Associate III

HI~~

I test camera STM32H743.

When I enable D cache(​(SCB_EnableDCache ())),camera image breaking phenomenon.

When I disable D cache(​(SCB_EnableDCache ())),it is working well.

=======================================================================

int main(void)

{

Frame_Buffer = RAM_START; -> external memory : 0x68000000 size : 0x25800(320*240*2)

MPU_Config();

SCB_EnableICache();

SCB_EnableDCache();

MX_DMA_Init();

MX_DCMI_Init();

HAL_DCMI_Start_DMA(&hdcmi, DCMI_MODE_CONTINUOUS, (uint32_t)Frame_Buffer, 76800);

}

void MPU_Config(void)

{

HAL_MPU_Disable()

MPU_InitStruct.Number = MPU_REGION_NUMBER4;

MPU_InitStruct.Enable = MPU_REGION_ENABLE;

MPU_InitStruct.BaseAddress = 0x68000000;

MPU_InitStruct.Size = MPU_REGION_SIZE_256KB;

MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;

MPU_InitStruct.IsBufferable = MPU_ACCESS_BUFFERABLE;

MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;

MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;

MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL2;    // = DEVICE

MPU_InitStruct.SubRegionDisable = 0x00;

MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;

HAL_MPU_ConfigRegion(&MPU_InitStruct);

HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);

}

===========================================================================

Let me know how to relsove this issue~~~

Please~~

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.