2018-07-27 5:10 AM
Currently I'm trying to get CAN up and running on a STM32F469NIH6 based Board using the CubeMX libraries.
Unfortunately, the documentation of the new HAL_CAN driver is very limited. I found an example in STM32Cube_FW_L4_V1.12.0\Projects\STM32L476G-EVAL\Examples\CAN\CAN_Networking\Src\main.c, but even with identical code (except the clock settings), it is not working, because the frame I added with HAL_CAN_AddTxMessage(&hcan1, &txHeader, data, &txMailbox) is not being sent, possibly because of the HAL_CAN_STATE_LISTENING.
My RX and TX lines (to the CAN-Transceiver) are both in HIGH-State (3.3V) and they keep being there when trying to transmit. CAN_H and CAN_L itself is in High-Z state, both lines are around 2V, Vdiff = 0V
Is there anything I can do wrong? Any suggestions how to debug this down to the problem?
2018-07-27 5:15 AM
Are you running a line driver with a terminator ?
is there another device on the canBus ?
2018-07-27 5:18 AM
Yes, both ends are terminated with 120 Ohms and I run with a ISO1050 Transceiver from Texas.
Yes, there is another devices, that sends something when I switch the system on.
I have some very old firmware running on that board (using the old ST Standard Libraries), that where able to send something.
2018-07-27 5:47 AM
I use this method to transmit.. checking all three mailboxes manually.
if ((CAN->TSR & CAN_TSR_TME0) == CAN_TSR_TME0) // (1)
{
CAN->sTxMailBox[0].TDTR = canTxMsgLength[canTxMsgOUT]; // (2) length
CAN->sTxMailBox[0].TDLR = canTxMsgBottomWord[canTxMsgOUT]; // (3) 4bytes
CAN->sTxMailBox[0].TDHR = canTxMsgTopWord[canTxMsgOUT]; // (3) 4bytes
CAN->sTxMailBox[0].TIR = ((uint32_t)canTxMsgID[canTxMsgOUT] << 21 | CAN_TI0R_TXRQ); // (4) // send it now if the line is idle
}
if ((CAN->TSR & CAN_TSR_TME1) == CAN_TSR_TME1) // (1)
if ((CAN->TSR & CAN_TSR_TME2) == CAN_TSR_TME2) // (1)
2018-09-20 12:26 AM
I have the same problem with my STM32F437ZI
@themole cuold you solve it?
Can somebody solve the topic with the HAL interface?
2018-09-24 4:13 AM
I have some time the same probleme. It works for a long time after but some times, Tx buffers become full. After a reset, all is working fine without any change in term of hardware. So I should solve this issue with software.
I check if tx mailbox are full with HAL_CAN_GetTxMailboxesFreeLevel(pcan);
If not, I clear wiht this HAL_CAN_AbortTxRequest(pcan, 0); HAL_CAN_AbortTxRequest(pcan, 1); HAL_CAN_AbortTxRequest(pcan, 2); but it not solved or partialy ( the fault occurence is less)
The fact that the state in HAL_CAN_SATE_LISTENING seems to not be the issue.
Thanks for your advise.
Bertrand
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.