2025-06-14 10:14 AM
I am trying to run the Secure Boot examples from STM32CubeL5 and have everything built, but on step 2 where I run `TFM_SBSFU_Boot\STM32CubeIDE\regression.sh` I am having an error where I cannot program the option bytes.(Another similar thread was with someone who bought a counterfeit part so I'll also mention that I bought the kit from ST.)
This is the script output
$ ./regression.sh
regression script started
Regression to RDP 0, enable tz
-------------------------------------------------------------------
STM32CubeProgrammer v2.19.0
-------------------------------------------------------------------
ST-LINK SN : 004600313137510B33333639
ST-LINK FW : V3J13M4
Board : STM32L562E-DK
Voltage : 3.29V
SWD freq : 8000 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x472
Revision ID : Rev Z
Device name : STM32L5xx
Flash size : 512 KBytes (default)
Device type : MCU
Device CPU : Cortex-M33
BL Version : --
UPLOADING OPTION BYTES DATA ...
Bank : 0x00
Address : 0x50022040
Size : 40 Bytes
[==================================================] 100%
Bank : 0x01
Address : 0x50022060
Size : 16 Bytes
[==================================================] 100%
PROGRAMMING OPTION BYTES AREA ...
Warning: Option Byte: rdp, value: 0xAA, was not modified.
Warning: Option Byte: tzen, value: 0x1, was not modified.
Warning: Option Bytes are unchanged, Data won't be downloaded
Time elapsed during option Bytes configuration: 00:00:00.003
Remove bank1 protection
-------------------------------------------------------------------
STM32CubeProgrammer v2.19.0
-------------------------------------------------------------------
ST-LINK SN : 004600313137510B33333639
ST-LINK FW : V3J13M4
Board : STM32L562E-DK
Voltage : 3.29V
SWD freq : 8000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x472
Revision ID : Rev Z
Device name : STM32L5xx
Flash size : 512 KBytes (default)
Device type : MCU
Device CPU : Cortex-M33
BL Version : --
Hard reset is performed
UPLOADING OPTION BYTES DATA ...
Bank : 0x00
Address : 0x50022040
Size : 40 Bytes
[==================================================] 100%
Bank : 0x01
Address : 0x50022060
Size : 16 Bytes
[==================================================] 100%
PROGRAMMING OPTION BYTES AREA ...
Warning: Option Byte: secwm1_pend, value: 0x0, was not modified.
Warning: Option Byte: wrp1a_pend, value: 0x0, was not modified.
Warning: Option Byte: wrp1b_pend, value: 0x0, was not modified.
Bank : 0x00
Address : 0x50022040
Size : 40 Bytes
Reconnecting...
Reconnected !
UPLOADING OPTION BYTES DATA ...
Bank : 0x00
Address : 0x50022040
Size : 40 Bytes
[==================================================] 100%
Bank : 0x01
Address : 0x50022060
Size : 16 Bytes
[==================================================] 100%
OPTION BYTE PROGRAMMING VERIFICATION:
Error: Expected value for Option Byte "secwm1_pend": 0x0, found: 0x75
Error: Expected value for Option Byte "secwm1_pstrt": 0x7F, found: 0x0
Error: Expected value for Option Byte "wrp1a_pend": 0x0, found: 0x23
Error: Expected value for Option Byte "wrp1a_pstrt": 0x7F, found: 0x4
Error: Option Byte Programming failed Or modified by application after OB_LAUNCH
Time elapsed during option Bytes configuration: 00:00:02.122
regression script failed, press a key
If I open STM32CubeProrammer and edit the fields manually I get the same errors.
12:35:55 : UPLOADING OPTION BYTES DATA ...
12:35:55 : Bank : 0x00
12:35:55 : Address : 0x50022040
12:35:55 : Size : 40 Bytes
12:35:55 : Bank : 0x01
12:35:55 : Address : 0x50022060
12:35:55 : Size : 16 Bytes
12:35:55 : OPTION BYTE PROGRAMMING VERIFICATION:
12:35:55 : Error: Expected value for Option Byte "SECWM1_PEND": 0x0, found: 0x75
12:35:55 : Error: Expected value for Option Byte "WRP1A_PEND": 0x0, found: 0x23
12:35:55 : Error: Option Byte Programming failed Or modified by application after OB_LAUNCH
12:35:55 : Time elapsed during option Bytes configuration: 00:00:02.124
12:40:06 : Disconnected from device.
I'm not sure where to go from here to debug this. I have tried this on Windows and Linux with the exact same results so I don't think its a problem with my host tools.
2025-06-15 2:05 PM
Hello @dberliner ,
Perform a Full chip erase under the "Erase & Programming" tab. Then, reset the board and try running the code again. How to program STM32 Option Bytes with the HAL API - STMicroelectronics Community
2025-06-18 1:34 PM
When I try to run a full chip erase I get:
15:07:08 : MASS ERASE ...
15:07:08 : Error: failed to erase memory
15:07:08 : Error: Mass erase operation failed.Please verify flash protectionSame results when I try connecting under reset.
2025-06-23 1:36 AM
Check the power supply and that the target voltage is stable.
2025-06-23 7:16 AM
I'm using the USB port and have tried several cables directly plugged into the USB ports on my PC. I need to find some wires for my bench supply so I'll update with that when I'm able. I dont have anything more complex than a multimeter to verify voltage but short of a hardware defect this shouldn't be an issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.