2022-02-26 5:47 AM
Hello,
I'm using a Nucleo board (NUCLEO-G070RB) with STM32F103RB MCU and I try to use channel 11 of ADC1 mapped to PC1 to get values from a humidity sensor. I noticed that the values are invalid and it's not because of the sensor.
I created a sample application and connected PC1 to VCC but the values are about 2000 instead of 4095. When I connect to GND I get same values instead of 0.
Here is the code:
#include "stm32f103xb.h"
uint32_t adcValue = 0;
int main(void)
{
/* Enable GPIOC clock */
RCC->APB2ENR |= (1U<<4);
/* Configure PC1 to analog input */
GPIOC->CRL &= ~(1U<<4); // MODE1[0]: 0
GPIOC->CRL &= ~(1U<<5); // MODE1[1]: 0 input mode
GPIOC->CRL &= ~(1U<<6); // CNF1[0]: 0
GPIOC->CRL &= ~(1U<<7); // CNF1[1]: 0 analog mode
#if 0
/* Enable GPIOA clock */
RCC->APB2ENR |= (1U<<2);
/* Configure PA1 to analog input */
GPIOA->CRL &= ~(1U<<4); // MODE1[0]: 0
GPIOA->CRL &= ~(1U<<5); // MODE1[1]: 0 input mode
GPIOA->CRL &= ~(1U<<6); // CNF1[0]: 0
GPIOA->CRL &= ~(1U<<7); // CNF1[1]: 0 analog mode
#endif
/* Enable ADC1 clock */
RCC->APB2ENR |= (1U<<9);
/* Set channel 11 for ADC1 */
ADC1->SQR3 = 11U;
#if 0
/* Set channel 1 for ADC1 */
ADC1->SQR3 = 1U;
#endif
/* Set number of conversions */
ADC1->SQR1 = 0; // L[3:0]: 0000 -> 1 conversion
/* Enable ADC1 */
ADC1->CR2 |= (1U<<0); // set ADON to 1
/* Enable continuous mode */
ADC1->CR2 |= (1U<<1); // set CONT to 1
/* Set start software flag */
ADC1->CR2 |= (1U<<22); // set SWSTART to 1
/* Set ADON again to start conversion */
ADC1->CR2 |= (1U<<0); // set ADON to 1
while(1)
{
/* Check EOC bit for end of conversion */
while(!(ADC1->SR & 2U));
/* Read conversion value */
adcValue = ADC1->DR;
}
}When I use PA1 with channel 1 then values are correct (4095 or 0).
What can be the issue ?
Thanks.
Solved! Go to Solution.
2022-02-26 7:10 AM
Regardless, you could set PC1 as an output and see that you can measure it with a multimeter to verify correct hardware pinout. Or as an input and verify that IDR reads correctly.
You should also verify the register settings are correctly set by examining them in a debugger. Technically you need a delay of a few cycles between enabling a clock and using it. This may be preventing the "ADC1->SQR3 = 11U" line from happening.
2022-02-26 6:59 AM
> I'm using a Nucleo board (NUCLEO-G070RB) with STM32F103RB MCU
How, exactly? They don't have compatible pinouts.
2022-02-26 7:10 AM
Regardless, you could set PC1 as an output and see that you can measure it with a multimeter to verify correct hardware pinout. Or as an input and verify that IDR reads correctly.
You should also verify the register settings are correctly set by examining them in a debugger. Technically you need a delay of a few cycles between enabling a clock and using it. This may be preventing the "ADC1->SQR3 = 11U" line from happening.
2022-02-26 7:26 AM
I'm using following board user manual: STM32 Nucleo-64 boards (MB1360) - User manual and in this document board name is referenced as I mentioned above. I checked my board and actually is NUCLEO-F103RB.
Configuration of connectors and pins are similar with my board.
2022-02-26 9:15 AM
Thank you for suggestions.
I configured PC1 in output mode, toggling ODR register each second and I connected a logic analyzer to the pin. Signal is flat, not as expected.
I used same code but configured for PA1 and the output is as expected.
I don't understand why same code works for PA1 (as output and input from ADC1) but not for PC1.
I verified register settings when testing PC1 in debug mode and all registers are set correctly.
I put a delay of 1ms after setting the channel but still not working.
2022-02-26 9:26 AM
I found the problem.
I used the wrong user manual for board :unamused_face:
I downloaded the right document and I noticed the PC1 is located on a different connector. It's working now.
Thank you @TDK for your help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.