2020-04-17 8:45 AM
2020-04-17 10:23 AM
No it is not.
If you want ucLinux, try emcraft.com
2020-04-17 6:28 PM
Thank you very much for the response. Will check @ emcraft.com. Do ST provide any other OS and drivers for STM32F407VG MCU board? I understand that there are various work bench options available though.
2020-04-17 7:41 PM
Which board specifically? The discovery board?
CubeF4 contains peripheral examples.
Examples of FreeRTOS.
Not really enough memory and MMU to support Embedded Linux.
You're going to need bare metal skills to much productive with these MCU
2020-04-18 2:59 AM
The board is STM32F4DISCOVERY. Thanks for providing the references. will explore CubeF4.
2020-04-20 5:32 AM
In CubeF4 1.25.0, i see that user manuals for HAL drivers are starting from STM32F410Rx, 411xE and so on. I certainly think that the HAL is supported for USB Device functionality for STM32F4DISCOVERY board which has STM32F407VG MCU. Please let me know if my assumption is fine.
Also, can you please suggest me any USB class device driver for streaming functionality?
Thanks in advance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.