2017-05-18 12:45 AM
Hi,
I use a Nemeus pico gateway and a B-L072Z-LRWAN1 with the I-CUBE-LRWAN software.
I displayed uplink message with a python scrypt running on a Raspberry Pi.
Nevertheless, i can't see downlink message like the join accept message.
How can i fixed this problem? I have to change something in the end node program of I-CUBE?
Thanks in advance
2017-05-23 6:31 AM
Hi
forget.maxence
,Do you still face the reported issue?
Is it related to the one reported in
https://community.st.com/0D70X000006SsLLSA0
which is already fixed?Please keep us informed.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-05-24 2:05 AM
Hello,
The problem is not fixed. My purpose is to see frame during the join procedure or to see ACK message. Is it possible? Should i modify the code of my device or is it a gateway problem?
Thanks in advance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.