2014-09-29 2:16 PM
Hi all,
I've been getting familiar with the RCC stuff on the STM32L152 (STMrecently152L-Discovery), but I'm struggling to push the baud rate of my USART transmission beyond 130Kbaud. I've set up the SysClk to use the PLL, after dividing the HSI down to 12MHz (16MHz*3/4). That's far faster than the default 2MHz it was running on before so seems to me like it should be plenty headroom for the USART to be able to up its speed. What I'm seeing though when I set the Baud to > 130Kbps though is the actual Baud rate dropping to near 200bps on the scope. I'm not sure if there's a stage of configuration I'm missing, but I think I've been looking at it so long I wouldn't even be able to spot it now. I know my clock config is working okay in terms of the SYSCLK, because setting up my MCO pin using the SYSCLK will output the expected 12MHz.RCC_MCOConfig(RCC_MCOSource_SYSCLK,RCC_MCODiv_1);
Clock configuration:
/* Configure the clocks as required */
void
Clock_cfg(
void
){
// Enable HSI //
RCC_HSICmd(ENABLE);
// Enable Prefetch Buffer //
FLASH_PrefetchBufferCmd(ENABLE);
// Flash 0 wait state //
FLASH_SetLatency(FLASH_Latency_0);
// HCLK = SYSCLK // HCLK derived from SCLK
RCC_HCLKConfig(RCC_SYSCLK_Div1);
// APB1 Clock
RCC_PCLK1Config(RCC_HCLK_Div1);
// APB2 Clock
RCC_PCLK2Config(RCC_HCLK_Div1);
// Set PLL clock as HSI*8/4 = 16MHz/2
RCC_PLLConfig(RCC_PLLSource_HSI, RCC_PLLMul_3, RCC_PLLDiv_4);
// Enable PLL
RCC_PLLCmd(ENABLE);
// Wait til PLL is ready
while
(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET);
// SysClk/AHB clock config // Set from PLL Clock
RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK);
// Wait till PLL is used as system clock source
while
(RCC_GetSYSCLKSource() != 0x0C);
}
USART config:
// Configure pin for USART TX
GPIO_IS.GPIO_Pin = USART_TX;
// Configure pin
GPIO_IS.GPIO_Mode = GPIO_Mode_AF;
// Set as output
GPIO_IS.GPIO_OType = GPIO_OType_PP;
// Push/pull
GPIO_IS.GPIO_Speed = GPIO_Speed_40MHz;
// 40MHz clk
GPIO_IS.GPIO_PuPd = GPIO_PuPd_UP;
// Pull-up
GPIO_Init(USART_PORT, &GPIO_IS);
// Configure alternate functions
GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_USART2);
// PA2 - USART2_TX
// Configure USART
USART_IS.USART_BaudRate = 140000;
USART_IS.USART_WordLength = USART_WordLength_8b;
USART_IS.USART_StopBits = USART_StopBits_2;
USART_IS.USART_Parity = USART_Parity_No;
USART_IS.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_IS.USART_Mode = USART_Mode_Tx;
//Apply structure
USART_Init(USART2, &USART_IS);
// Enable USART
USART_Cmd(USART2, ENABLE);
Any advice or ideas would be very welcome!
#usart-rcc-clock-frequency-baud
2014-09-29 5:46 PM
You should be attentive to what the APB clocks are, as the peripheral, and it's baud clock, come from there.
A bus running at 12 MHz could achieve 130435 baud with a 130kbaud programmed rate, the error coming from the achievable division.2014-09-29 11:36 PM
Perhaps I'm being naive here, but surely before I changed my clock speed and assigned the SYSCLK the PLL's 12MHz, it and all my other clocks would be running at 2MHz from the MSI? At this point I was managing to get 130Kbaud from my USART too. As far as I can see I've set the source of my HCLK (AHB clock) as the SCLK.
I should be clear that my end goal here is to be able to drive the USART at 250Kbps in order to transmit DMX512 packets. The problem I'm experiencing is that I can't drive it faster than 130Kpbs despite having increased (at least I think I have) the AHB and APB1 clocks.What else could the problem be? How can I go about debugging this more than I already have?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.