2018-01-06 4:39 AM
Hi folks,
I'm trying to initialise system clock to 168MHz without using cubemx generated function just to get better grasp of the RCC , PLL and clocks. So currently I'm trying to use HSE as source for PLL and PLL out as System core clock, right after setting the clock switch bits in RCC->CFGR, controller crashes.
Attached below is the function.
#stm32-f4 #clock #crash #pll #rcc2018-01-06 7:48 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.