2019-11-28 12:24 AM
2019-11-28 12:46 AM
How about checking the datasheet: https://www.st.com/resource/en/datasheet/st8500.pdf ?
2019-11-28 4:01 AM
Ya I have checked but it lacks clarity.They haven't directly mentioned it supports communication through DC line.
2019-11-28 4:50 AM
DC to 500 KHz
Probably would have lead with something clearer in front page bullets.
2019-11-28 4:55 AM
Thank you. I did see that. DC with what voltage???
2019-11-28 5:46 AM
Would suggest you talk with an FAE supporting the Power Line Comms products.
I'd presume it would connect via a DC blocking capacitor. The ADC has a 1.8V p-p range
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.