2021-02-26 12:30 PM
(This is regarding STM32H75x)
SRAM1, SRAM2, and SRAM3 are separate in the memory map, but they are continuous - there are no gaps between them:
Can they be treated as continuous with respect to the linker, for example:
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288KAnd then place some arbitrary data in that region?
Like, can we place an array that is 288k in that region and use it as a heap, or will bad things happen at the region where SRAM1 ends / SRAM2 starts, etc?
2021-03-12 9:56 AM
I feel like there is a simple answer to this but I haven't been able to find it...
2021-03-12 10:01 AM
From the processors perspective they look/appear contiguous.
From and DMA/BUS perspective they might be treated differently, you'd have to review in the context of the bus matrix diagrams
Clocks should also be enabled.
2021-03-12 10:29 PM
To use as heap, they're contiguous and the linker doesn't care what they, read https://sourceware.org/binutils/docs/ld/MEMORY.html#MEMORY.
SRAM123 (rw) : ORIGIN = 0x30000000, LENGTH = 0x48000Otherwise find your part's RM and other resources, e.g. AN4891, at https://www.st.com/content/st_com/en/search.html.
2021-03-13 3:06 PM
If this is relevant for your application, test whether multi-byte writes over the boundary of the RAMs don't cause trouble.
For example: *(uint32_t *)(0x3003FFFF) = 0x12345678; *(uint32_t *)(0x3001FFFE) = 0x12345678;
-- pa
2021-03-15 8:19 AM
Thanks everyone.
One interesting thing: I did not realize that clocks had to be enabled for these SRAM blocks, and I was somehow using them just fine without those clocks enabled.
I am not sure how... but I have added the clock init in.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.