2021-09-30 5:06 PM
Hi,
I am using STM32F746G_DISCO board to create different pages for the LCD. I see only one page with 4 tabs project already takes 300KByte flash memory code space. The STM32F746 only has 1MByte flash. So I like to store the LCD graph code related modules to QSPI NOR flash on the discovery board and store other portions of firmware in STM32 flash. I see the QSPI_ExecuteInPlace example copies the .qspi section from LMA to VMA, then run from VMA(in QSPI flash). But the .qspi section also occupy the MCU internal flash space. Is there a way I can move section from internal to external flash, not copy?
The question is internal 1Mbytes flash is not enough to handle a few LCD pages plus other functionalities. In this case, how to use QSPI flash to share the load for program code space?
2021-09-30 6:06 PM
The linker script / scatter file needs an actual QSPI memory region, at 0x90000000, and you need to direct content into that region rather than the internal memory region.
STM32Cube_FW_F7_V1.15.0\Projects\STM32746G-Discovery\Examples\QSPI\QSPI_PreInitConfig\SW4STM32\STM32746G-DISCOVERY\STM32F746NGHx_FLASH.ld
2021-10-04 6:15 AM
Thank you, Tesla.
In the QSPI_PreInitConfig example, how to put const array data to QSPI flash? I try to declare as follows, but cannot pass compiler. error: 'img2' causes a section type conflict with 'GpioToggle'
__attribute__((section(".qspi")))
const unsigned char img2[2] =
{
0xFF, 0xFF
};
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.